Redundancy-RSTP Bridge
Description
The page displays the diagnostic data of RSTP bridge.
The users with Installer or Engineer roles can consult the Diagnostics pages.
Navigation to the Redundancy-RSTP Bridge Page
To view the page, click .
General Parameters
|
Parameter |
Description |
|---|---|
|
|
Status of RSTP feature. It is either enabled or disabled based on the configuration. |
|
|
Unique identifier of this Bridge. It is a combination of MAC address and Bridge Priority of this device. |
|
|
Unique identifier of the Root Bridge. Combination of MAC address and Root Bridge Priority of the Root device |
|
|
The port number that offers the lowest cost path from this bridge to the root bridge. NOTE: For the Root Bridge, the value is always 0. For other
devices, either 1 or 2.
|
|
|
The cost of the path to the root as seen from this bridge. |
|
|
Total number of topology changes detected by this bridge since the last reset counters. |
|
Click to reset the statistics values to 0. If the IFE interface is switched off or if it is reset due to a configuration change or another event, the statistics values are reset to 0. |
|
Configured/Learned Parameters
|
Parameter |
Description |
|---|---|
|
|
The value of Hello Time configured at this Bridge. |
|
|
The actual Hello Time used by the bridge currently. This is the configured Hello Time of the Root Bridge. |
|
|
The value of Forward Delay configured at this Bridge. |
|
|
The actual Forward Delay used by the bridge currently. This is the configured Forward Delay of the Root Bridge. |
|
|
The value of Max Age Time configured at this Bridge. |
|
|
The actual Max Age Time used by the bridge currently. This is the configured Max Age Time of the Root Bridge. |