0602IB1801EN-09

IO Readings

Description

The IO Readings page shows the IO module input/output configuration. It displays six digital inputs, three digital outputs, and one analog input. The IO application control is possible only when the IO module is connected to a circuit breaker.

The table shows the steps to access the IO Readings page:

Step

Action

Result

1

From the IFE menu bar, click Diagnostics .

Opens the Diagnostics page.

2

From the Diagnostics menu, select the circuit breaker from IO Readings submenu.

Opens the IO Readings page for the circuit breaker.

List of Parameters in IO Module

Parameter

Description

Setting

Inputs

Displays the six digital inputs configured in the IO module.

Outputs

Displays the three digital outputs configured in the IO module.

Analog Inputs

Displays the analog input assigned in the IO module.

Label

Displays the assigned functions of the corresponding inputs or outputs.

Value

Displays the value of the six digital inputs and three digital outputs

  • 1

  • 0

Force/Unforce

Displays the six digital inputs and three digital outputs are forced or unforced

  • UNFORCED

  • FORCED

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?