Read Device Registers
Description
Read device registers allows the IFE interface to read Modbus registers from the devices connected to the ULP port of the IFE interface.
Read Procedure
|
Step |
Action |
Result |
|---|---|---|
|
1 |
From the IFE menu bar, click . |
Opens the menu. |
|
2 |
From the menu, in the submenu, click . |
Opens the page. |
|
3 |
From the , select the device. |
Selects the device from the drop-down list. |
|
4 |
Enter (or choose from the defined device list), , and the to read. |
Enters the registers to read from the specified device. |
|
5 |
Select the data type from drop-down list. |
Selects the appropriate data type. |
|
6 |
To change how Modbus data is displayed in the column, select , , , or . |
Selects how the data values are displayed. |
|
7 |
Click . |
Reads the device registered according to the selected configuration. |
IFE Read Device Register Parameters
|
Parameter |
Description |
Settings |
|---|---|---|
|
|
Selects a device to read from the list of previously added devices. |
– |
|
|
The address (local ID) of the device that is to be read. |
1 |
|
|
Register number in decimal. |
0–65535 Default setting: 1000 |
|
|
The number of registers to read. |
1–125 Default setting: 10 |
|
|
Lists the register numbers in decimal. |
– |
|
|
Lists the data stored for a register. Values retrieved depend on the device connected to the IFE interface. Refer to the documentation for the connected device for more information about stored register values. |
– |
|
|
Lists the data types available for the device. |
|
|
|
Select an option to specify how the value column data is displayed. |
(Default setting) |