Webpage Description
Webpage
Webpage
|
Submenu |
Webpage |
Description |
|---|---|---|
|
|
Displays diagnostic data used to troubleshoot the network-related problems. |
|
|
Displays the diagnostic data of Ethernet global statistics and Ethernet port characteristics. |
||
|
Displays the global statistics of TCP/IP and TCP port connections. |
||
|
Displays the global statistics of ULP port connection. |
||
|
Displays the diagnostic data of RSTP bridge. |
||
|
Displays the diagnostic data of RSTP ports. |
||
|
Displays the diagnostic data of SNMPV1 Agent. |
||
|
– |
|
|
|
|
|
Webpage
|
Submenu |
Webpage |
Description |
|---|---|---|
|
|
Sets the date and time manually or sets the IFE time automatically using an NTP source or configures the device connected to IFE interface to synchronize their time with the IFE time automatically. |
|
|
Sets the time zone for the region and sets the daylight saving time. |
||
|
Sets IFE preferences for data refreshment. |
||
|
|
Sets the Modbus TCP/IP communication interface. |
|
|
Sets the IP parameters. |
||
|
Sets the configuration of SMTP server for mailing purpose. |
||
|
Sets data generation and publishing parameters. |
||
|
Sets the RSTP bridge and RSTP port details. |
||
|
Sets the SNMPV1 agent parameters. |
||
|
- |
|
|
|
|
|
Webpage
|
Submenu |
Webpage |
Description |
|---|---|---|
|
- |
Configures the settings and activates the IP network services. |
|
|
- |
Configures the IP addresses that can access the IFE interface through Modbus TCP/IP. |
|
|
- |
Displays the IFE certificate with expiration date and validity period. |
|
|
- |
Manages the existing and newly added user accounts. |
|
|
- |
Configures the Syslog server address. |