7EN02-0423-03

Reset

You can reset logs and trends. Further, you can perform factory reset.

You can access the device reset parameters by selecting Menu > Settings > Reset.

The reset parameters are Reset Logs, Reset Trend, and Factory Reset.

On performing reset of logs or trends, the existing logs or trend information is erased but the settings parameter value remains unchanged. On performing factory reset, the settings parameter values are reset to default.

The complete list of settings parameters, its default value, and allowed values are:

The following table is profiled. Check for row profiling before making any content change.
Parameter Default Value Allowed Values
Ins. Alarm 1 kΩ 0.04…500 kΩ
Ins. Al. Delay 0 s 0 s...120 minutes
Prev. Alarm OFF
  • 1 kΩ...1 MΩ
  • OFF
Prev. Al. Del 0 s 0 s...120 minutes
Disconnect. Inj OFF
  • ON

  • OFF

App

IM400N:Power C

IM400THRN: THR

IM400N:

  • Power C

  • Control C

IM400THRN: THR

Filtering

IM400N:40s

IM400THRN: 20s

IM400N:

  • 4s

  • 40s

  • 400s

IM400THRN:

  • 2s

  • 20s

  • 200s

Locating *

Alarm

  • OFF

  • Prev.Al.

  • Alarm

  • IFL

V.Adapt

IM400N:None

IM400THRN: P1N

IM400N:

  • None

  • VA2

  • PHT1000

  • HV1700

IM400THRN:

  • None

  • P1N

Frequency *

50 Hz

  • 50 Hz

  • DC

  • 400 Hz

  • 60 Hz

HRG

OFF

  • OFF

  • 0.1....2 MΩ

Injection *

20V

  • 20V

  • 40V

  • 60V

  • 80V

Pri.DC Resis *

0 kΩ

0....50 kΩ

No. of Transfo *

0

  • 0

  • 1

  • 3

Ins. Al. Relay FS
  • Std.

  • FS

Prev. Al. Rel FS
  • Std.

  • FS

  • Mirror

Inhibit. Input N.O.
  • N.O.

  • N.C.

  • OFF

Ack Inhibit OFF
  • ON

  • OFF

Ack Al. Relay ON
  • ON

  • OFF

Corr. Flt. Signal OFF
  • ON

  • OFF

Test w. Relays ON
  • ON

  • OFF

Inhibition Type Int.
  • Int.

  • Ext.

Address 1 1...247
Auto Config OFF
  • ON

  • OFF

Baudrate 19200
  • 4800

  • 9600

  • 19200

  • 38400

Parity Even
  • None

  • Even

  • Odd

Modify Password 0000 0000...9999
Activation (Password) OFF
  • ON

  • OFF

Contrast 50% 10...100%
Backlight 100% 10...100%
Screen Saver OFF
  • ON

  • OFF

QR code for this page

Was this helpful?