Homeline Ground-Fault Circuit Breakers (HOM-GFI)

Homeline Ground-Fault Circuit Breakers (HOM-GFI)

HOM 1P GFI
(With Ground Fault
Circuit Interrupter)
1 Space Required

HOM 2P GFI
(With Ground Fault
Circuit Interrupter)
2 Spaces Required

HOM-GFI circuit breakers provide overload and short circuit protection, combined with Class A ground fault protection. Class A denotes a ground fault circuit interrupter that will trip when a fault current to ground is 6 milliamperes or more.

HOM-GFI Circuit Breakers

Circuit Breaker Type

Ampere
Rating 

AIR

1P—120 Vac
1 Space Required

2P—120/240 Vac
Common Trip
2 Spaces Required

Ground-Fault Circuit Interrupter(Pigtail Neutral)

15 A

10 kA

HOM115GFI

HOM215GFI

20 A

10 kA

HOM120GFI

HOM220GFI

25 A

10 kA

HOM225GFI

30 A

10 kA

HOM230GFI

35 A

10 kA

HOM235GFI

40 A

10 kA

HOM240GFI

45 A

10 kA

HOM245GFI

50 A

10 kA

HOM250GFI

Plug-On Neutral Ground-Fault Circuit Interrupter

15 A

10 kA

HOM115PGFI

20 A

10 kA

HOM120PGFI

Feedback