Binary Input objects
The following table lists the Binary Input (BI) objects available on the meter.
Object ID | Object name | Description |
---|---|---|
38416, 38417 |
Digital Input 1 Digital Input 2 |
Status of digital inputs 1 and 2:
NOTE: This information only applies if the digital input
is configured as a status input.
|
38448, 38449 |
Digital Output 1 Digital Output 2 |
Status of digital outputs:
|