EAV15107-EN11

Firmware upgrades

The power meter supports the downloading of new firmware and language files over the communications link.

This requires the free DLF3000 software, which is available at www.se.com . The DLF3000 offers an extensive Help file with information on operating the software. The most recent firmware and language files are also available on the website.

QR code for this page

Was this helpful?