EAV15107-EN10

Power quality measurements

The meter provides harmonic distortion metering up to the 31st harmonic.

The following power quality measurements are available:

  • Individual harmonics (odd harmonics up to 31st)

  • Total harmonic distortion (THD, thd) for current and voltage (line-to-line, line-to-neutral)

  • Total demand distortion (TDD)

The following harmonics data is available on the display:

  • Numeric magnitude and angle of the fundamental (first) harmonic.

  • Graphical display of the 3rd to 31st harmonics, expressed as a percentage of the fundamental harmonic.

QR code for this page

Was this helpful?