EAV15107-EN11

Setting the clock using the display

The Clock setup screens allow you to set the meter’s date and time.
NOTE: You must always set or sync the meter time to UTC (GMT, Greenwich Mean Time), not local time. Use the GMT Offset (h) setup parameter to display the correct local time on the meter.
  1. Navigate to Maint > Setup .
  2. Enter the setup password (default is “0”), then press OK.
  3. Navigate to Clock .
  4. Move the cursor to point to the parameter you want to modify, then press Edit.
  5. Modify the parameter as required, then press OK.
  6. Move the cursor to point to the next parameter you want to modify, press Edit, make your changes, then press OK.
  7. Press the up arrow to exit.
  8. Press Yes to save your changes.
    Parameter

    Values

    Description

    Date

    DD/MM/YY

    MM/DD/YY

    YY/MM/DD

    Set the current date using the format displayed on screen, where DD = day, MM = month and YY = year.
    Time

    HH:MM:SS (24 hour format)

    HH:MM:SS AM or PM

    Use the 24-hour format to set the current time in UTC (GMT).
    Meter Time GMT, Local Select GMT if you set the current time to Greenwich Mean Time zone. Otherwise, select Local.
    GMT Offset (h) * ± HH.0 Available only when Meter Time is set to Local. Set the GMT Offset between ± 00.0 and ± 12.0

    To configure the clock using ION Setup , see the section for your meter in the ION Setup online help or in the ION Setup device configuration guide, available for download at www.se.com .

QR code for this page

Was this helpful?