EAV15107-EN11

Setting up the screen passwords

It is recommended that you change the default password in order to prevent unauthorized personnel from accessing password-protected screens such as the diagnostics and reset screens.

This can only be configured through the front panel. The factory-default setting for all passwords is “0” (zero).

If you lose your password, you must return the meter for factory reconfiguration, which resets your device to its factory defaults and destroys all logged data.

NOTICE
Irrecoverable password
Record your device's user and password information in a secure location.
Failure to follow these instructions can result in data loss.

  1. Navigate to Maint > Setup .
  2. Enter the setup password (default is “0”), then press OK.
  3. Navigate to HMI > Pass .
  4. Move the cursor to point to the parameter you want to modify, then press Edit.
  5. Modify the parameter as required, then press OK.
  6. Move the cursor to point to the next parameter you want to modify, press Edit, make your changes, then press OK.
  7. Press the up arrow to exit.
  8. Press Yes to save your changes.

    Parameter

    Values

    Description

    Setup

    0000 - 9999

    Sets the password for accessing the meter setup screens (Maint > Setup).

    Energy Resets

    0000 - 9999

    Sets the password for resetting the meter’s accumulated energy values.

    Demand Resets

    0000 - 9999

    Sets the password for resetting the meter’s recorded peak demand values.

    Min/Max Resets

    0000 - 9999

    Sets the password for resetting the meter’s recorded minimum and maximum values.

    Diagnostics

    0000 - 9999

    Sets the password for accessing the meter’s diagnostics screens.

QR code for this page

Was this helpful?