Dimming Curve
With the inbuilt load profiles, dimming curve relationship is linear. However, with some types of load dimming curve will result in a non-linear change with perceived brightness as you dim. In such case, a custom dimming curve can be defined to address.
Example: At low conduction time, a small change in conduction time
may result in a large change in brightness.
Since
C-Bus ramp rates give a constant rate of change of level and therefore
conduction time, this is perceived as very rapid dimming at the low
end and slower dimming at the high end. Using a dimming curve with
a flatter slope at the bottom end results in smaller changes in conduction
time in the lower dimming range, giving more control.
Min/Max Scaling
The Min/Max scaling feature takes the input control level range of 1-255 and scales it to the range Min-Max.
-
An input control level of 0 is always 0 (off)
-
An input control level of 1 is scaled to Min
-
An input control level of 255 is scaled to Max
For example, the kitchen and bedroom can use the same load profile since the load type is the same, but can adjust the range using the Min/Max scaling instead.