Compatible Loads
The C-Bus Digital Dimmers are compatible with a wide range of dimmable low-voltage lighting, as long as they operate within the specified channel ratings and built-in protection mechanisms.
|
Load Type |
Symbol |
Required Mode |
5508D1D Rating |
5504D2D Rating |
5504DHD Rating |
|
Dimmable LED Lamps and luminaries |
LED |
TE |
1 A |
2 A |
5 A* |
|
Incandescent/Halogen Lamps |
TE |
1 A |
2 A |
5 A* |
|
|
Dimmable Electronic Transformers with ELV Halogen Lamps, LED Lamps, or LED Strip** |
|
TE |
1 A |
2 A |
5 A* |
|
Dimmable Iron-Core Transformers with ELV Halogen or LED Lamps |
|
LE |
1 A |
2 A |
5 A* |
|
Dimmable LED Lamps and luminaries Dimmable Electronic Transformers with ELV Halogen Lamps, LED Lamps, or LED Strip (Special Cases***) |
LED
|
LE*** |
43 W 20 W 22 W 10
W |
86 W 40 W 43 W 20
W |
43 W 20 W 43 W 20
W |
*Total load across any 2 adjacent channels must be limited to 6 A / 1380 W (230 V) / 660 W (110 V). For more details, refer Flexible Loading.
** LED strip drivers are limited by inrush current. For more details, refer to the section Overcurrent Protection .
*** For more information, refer Using LE Mode with Electronic Loads.
| NOTICE |
|---|
|
RISK OF Equipment Damage
Failure to follow these instructions can result in equipment damage.
|
Using LE Mode with Electronic Loads
To utilise the full rating of the dimmer, Electronic/Capacitive load types such as LEDs must run in TE mode.
In some situations, such as where a ripple filter may be required upstream from the dimmer, it may be necessary to set the dimmer channels to LE mode, even when using a capacitive load such as an LED.
In such cases, the capacitive load creates a high inrush current at turn on every mains half-cycle, which significantly increases the power dissipation of the dimmer. In this configuration, the load rating is significantly reduced as per the table. The rating in this situation is also affected by the power factor of the load (which is an indication of the amount of capacitance it presents to the dimmer channel). Higher power factor is better, and load types with power factor lower than 0.8 should be avoided.