Project Design and Installation
Installation Requirements
-
Airflow around the unit and the ventilation holes must not be restricted.
-
Adequate ventilation should be provided in the enclosure to ensure that the temperature in the enclosure is maintained within the rated operating temperature range of the dimmer.
-
If the anticipated ambient temperature levels are higher than operating temperature, it is advised to refer the derating table guidelines to adjust the dimmer load accordingly. For more details, refer Operating Temperature and Derating.
-
The operating calorific values and the heat load must be considered when designing the distribution board.
-
Connect only compatible load types to the dimmer.
-
The use of external surge protection such as the Clipsal Max9 MX9SP140 or Schneider Electric Acti9 A9L16182 is recommended.