BQT2430700_03

Indicators

Unit Indicator

The unit indicator shows status related to the unit itself, such as the internal temperature, configuration issues, firmware update etc.

Action

LED Indication

Status

Green LED is ON

  • Unit powered.

  • C-Bus Power Supply enabled.

Yellow LED is ON

  • Unit powered.

  • C-Bus Power Supply disabled.

LED OFF

No power to device.

Red LED is ON

  • Unit powered.

  • Configuration error.

Slow Flash Red, Green

  • Internal temperature has exceeded over-temperature threshold.

  • C-Bus Power Supply enabled.

Slow Flash Red, Yellow

  • Internal temperature has exceeded over-temperature threshold.

  • C-Bus Power Supply disabled.

Override Flash Red, Green

  • Internal temperature has exceeded over-temperature threshold.

  • Override active, C-Bus Power Supply enabled.

Override Flash Red, Yellow

  • Internal temperature has exceeded over-temperature threshold.

  • Override Active, C-Bus Power Supply disabled.

Override Flash Off, Green

  • Override active.

  • C-Bus Power Supply enabled.

Override Flash Off, Yellow

  • Override active.

  • C-Bus Power Supply disabled.

Fast Flash, Green

Secondary firmware update in progress.

C-Bus Indicator

The C-Bus Indicator shows the status of the C-Bus Network voltage and communications. The colour of the indicator relates to the C-Bus Network communications status, whereas the state of the indicator (solid, flashing etc) relates the C-Bus Network voltage.

Action

LED Indication

Status

Solid(not flashing)

Regardless of color

C-Bus voltage OK.

Steady Flash

C-Bus voltage marginal (15-20 V).

Short Flash

C-Bus voltage critical (<15 V).

Red

No C-Bus clock detected, host online.

Green

C-Bus clock detected, host online.

Yellow

C-Bus clock detected, host offline.

Off

No C-Bus voltage present or unit not powered.

Channel Indicator

The channel indicators show the operating mode of the channel as well as providing feedback on any configuration changes or error conditions.

Action

LED Indication

Status

Short-press on the channel


(< 0.5 seconds)

Channel On, Leading Edge mode.

Channel On, Trailing Edge mode.

Slow Flash, Red

Channel shutdown due to incompatible load or mode error.

Off

Channel Off.

On, Red

Channel Offline, normally due to no mains supply to channel or dimmer channel firmware requiring an update.

Fast Flash, Red

Channel shutdown due to over current.

Fast Flash, Yellow

Channel shutdown due to over temperature condition.

Slow Flash, Yellow

Channel operating at reduced setting due to over temperature condition.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.