Safety Precautions
DANGER |
|---|
|
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
Failure to follow these instructions will result in death or serious injury.
|
WARNING |
|---|
|
INCORRECT C-BUS CABLE INSTALLATION
The C-Bus network cabling is classified as Separated Extra-Low
Voltage (SELV) wiring. To maintain this requirement, the approved
C-Bus cable must be used.
Failure to follow these instructions can result in death, serious injury, or equipment
damage.
|
| NOTICE |
|---|
|
Incorrect C-Bus installation location
To prevent the possibility of intentional or unintentional
interference with the configuration or operation of the C-Bus installation,
this equipment should be installed in a location with appropriate
access control.
Failure to follow these instructions can result in equipment damage.
|
| NOTICE |
|---|
|
Equipment Damage
Failure to follow these instructions can result in equipment damage.
|
Megger Testing
| NOTICE |
|---|
|
megger testing
Megger testing must never be performed on any cable while
connected to the product as it could degrade the performance of the
product and/or the network.
Failure to follow these instructions can result in equipment damage.
|
| NOTICE |
|---|
|
MAXIMUM LOAD RATINGS APPLY
Ensure that the number of lighting loads connected to
a single device does not exceed the maximum load rating of each channel.
Failure to follow these instructions can result in equipment damage.
|
DANGER
WARNING