BQT2430700_03

C-Bus Network Connection

Connection to the C-Bus network is made via one or both of the RJ45 connectors. The two RJ45 connectors are internally connected to allow the C-Bus network to be looped through the unit. See below illustration for pinouts and cable conductor assignments.

Use only C-Bus certified cable, which is identifiable by its pink sheath.

For C-Bus cable, refer:

  • Catalogue number: 5005C305B (solid)

  • Catalogue number: 5005C305BST (stranded)

Pin

Wire Colour

Compliance to TIA/EIA 568A wiring standard

Signal

1

Green & White

Remote ON

2

Green

Remote ON

3

Orange & White

C-Bus Negative (-)

4

Blue

C-Bus Positive (+)

5

Blue & White

C-Bus Negative (-)

6

Orange

C-Bus Positive (+)

7

Brown & White

Remote OFF

8

Brown

Remote OFF

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.