BQT2430700_03

Local Override

The channel indicator buttons on the front of the unit, toggle the corresponding channel on and off, providing a local override capability. This can be disabled in software. Each button illuminates when its respective channel is in the ON state. The channel indicator buttons perform different functions depending on how they are pressed.

A long-press on any channel indicator button for one second or more, returns all channels to the C-Bus Network level.

NOTE: Double short-press and long-press operations only apply when the unit/channel is in local override mode.

By default, any C-Bus commands received by the unit will override local toggle changes. In this case, only the channel associated with the received commands will revert to the C-Bus Network state. This option can be disabled in the software settings.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?