BQT2430700_03

Live Viewing of Monitored Data

The current values of each of the monitored conditions are visible in SpaceLogic C-Bus Commission when connected to the live network.

This is found under the Status section at the bottom of the Property Editor window.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?