Logic
The Logic feature allows the level of up to four additional Logic group addresses to be combined with the dimmer channel's primary group address to determine the final level that controls the dimmer channel's output level. There are four logic groups available in the dimmer unit, and each channel can be combined with any combination of these.
In dimmers, there are two logic functions available :
-
In MIN logic, the output level takes the minimum value of the primary lighting group and the states of all logic groups which that channel is configured to be combined with.
-
This is useful as a way of limiting the brightness at different times of day. The primary group can be used to control the level and state, and the logic group can be used to limit the brightness. For example, a schedule can set the logic group to a lower level after dark so that lights turned on during the night only come on at a low level. The schedule would then also set return the logic group level to maximum at sunrise so that the lights starts to function normally again.
-
-
In MAX logic, the output level takes the maximum value of the primary lighting group and the states of all logic groups which that channel is configured to be combined.