Mounting and Wiring
Mounting
The dimmer should only be installed horizontally on the mounting rails (type DIN EN 50022 TS 35) inside a distribution board.
Electrical Connection
DANGER |
|---|
|
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
Failure to follow these instructions will result in death or serious injury.
|
The dimmer units are capable of handling up to :
-
5508D1D : 8 A across 8 dimmed channels (1 A per channel)
-
5504D2D : 8 A across 4 dimmed channels (2 A per channel)
-
5504DHD : 12 A across 4 channels (maximum of 5 A on any channel, maximum 6 A total on any 2 adjacent channels)
When installing the units:
-
The dimmer unit requires mains power provided via the L/N/E connections at the top left, as well as power to the dimming banks (5508D1D /5504D2D) or dimmer channels (5504DHD) in order to operate the dimmer channels.
-
All terminals on the dimmer unit are suitable for cable up to 4 mm2 when using bare cable or 2 x 2.5 mm2 if using ferrules.
-
Make sure while terminating cables into the terminals, that no loose strands of copper fall into unit or enter any aperture other than the terminal.
-
The terminals require a PH1 Phillips driver or a 0.8 x 4 flat blade screwdriver.
-
Torque must not exceed 0.6 Nm when tightening terminal screws.
-
Rubber bungs are supplied for unused RJ45 connectors, to stop foreign bodies from entering the unit. Always install these bungs when the unit is mounted inside a mains rated enclosure.
110 V Electrical Wiring
To use the dimmer with a 110 V unit supply, break the T-Block terminal using a screw driver and connect a wire link between terminals.
WARNING |
|---|
|
EQUIPMENT DAMAGE HAZARD
Do not break T-Block terminal and/or insert a wire link
unless using the dimmer with 110 V unit supply voltage.
Failure to follow these instructions can result in death, serious injury, or equipment
damage.
|
| NOTICE |
|---|
|
EQUIPMENT DAMAGE HAZARD
When breaking the T-Block in the terminal, be careful
to not damage other terminal blocks.
Failure to follow these instructions can result in equipment damage.
|
Phase Independence
The 5508D1D and 5504D2D have two separate Dimmer Banks which each require separate Active and Neutral connections.
On these variants, each Dimmer Bank may be connected to a different phase.
The 5504DHD High Power Dimmer has independent Active and Neutral connections per channel, meaning each channel may be connected to any phase.
On all models, the Unit Power Supply may be connected to any phase.
For details refer, 8 channel dimmer.
DANGER
WARNING