BQT2430700_01

Warn Before Off

Warn before OFF is an optional courtesy feature of the Dimmer. It can be enabled by and Enabled Control Group and the duration can be set up to 15 min.

When a command is received from C-Bus, and when warn before OFF is set, the channel:

  • Does not immediately turn off

  • Initiates a warning, indicating that the light is about to turn OFF

  • Turns OFF after the preset warning time

NOTE: The warning consists of going to a pre-set level (1-100%) for a pre-set duration (1-15 minutes), before it turns off. If a second OFF command whilst the warning sequence is active, this will cause the channel to turn off immediately.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?