BQT2430700_03

Configuring the Device

Configuration and commissioning of the C-Bus unit is done by the C-Bus connection using the SpaceLogic C-Bus Commission software. To download the software click here.

The unit must be powered for configuration, however power may be provided by the USB-C connection for programming via C-Bus (without an energized mains connection).

NOTE: Dimmer channels will not be functional when powered solely from the USB-C connection.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?