BQT2430700_03

Confirming the Dimming Mode

The purpose of the Load Detection Mode and the Mode Confirmation process is to ensure compatibility of the selected dimming mode with the intended load type. If the mode confirmation is performed without the load attached or with a different load, subsequent operation in TE mode with some types of iron-core load types may cause damage to the dimmer channel.

As part of the initial installation, the correct mode for each channel must be confirmed.


Refer the below flow chart:

NOTE: If it is necessary to change from LE mode back to TE mode, hold the channel button for more than 10 seconds. Once done, Load Detection Mode is re-enabled, and the Mode Confirmation process must be repeated.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?