BQT2430700_03

Firmware Update

The C-Bus Digital Dimmers contain multiple microprocessors, all of which can be updated. From time to time, new firmware may be released to enhance performance or add new functionality. The SpaceLogic C-Bus Commission software will notify if a firmware update is required.

Firmware updates are performed using the SpaceLogic C-Bus Commission software, and require a connection to the USB-C connector on the front end of the dimmer.

All required firmware files will be included and authenticated as part of the latest SpaceLogic C-Bus Commission software release.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?