C-Bus Power Requirements
Adequate C-Bus Power Supply units must be installed or enabled to support the total consumption of all C-Bus devices connected to the C-Bus Network segment.
C-Bus Power Supplies are specially designed to share load when distributed around the C-Bus Network. To achieve this, the integrated C-Bus Power Supplies have an output impedance of approximately 32 Ω up to their maximum current of 200 mA. Once the maximum current is exceeded, the output impedance increases sharply to limit the current to a safe level in the event of a fault in the C-Bus Network wiring.
There must not be more than 2000 mA of total C-Bus Power Supply capacity enabled on a single C-Bus Network segment as this is the limit of the current carrying capacity of the C-Bus Network cable.
The dimmer unit includes a switchable inbuilt C-Bus Power Supply, which can supply up to 200 mA to the C-Bus Network when enabled. By default, the inbuilt Power Supply is disabled, but can be enabled (or disabled) via the front panel.
The SpaceLogic C-Bus Commission software provides you with information whether the inbuilt Power Supply is enabled or disabled in each unit, as well as a summary of the total network power capacity and consumption. This can be helpful in determining the Power Supply requirements of a particular network.
Enabling/Disabling the C-Bus Power Supply from the Front Panel
The integrated C-Bus Power Supply can be enabled or disabled via the front panel by performing a short press on the top right channel button whilst holding down the top left channel button to toggle the enabled state. After the desired setting for the C-Bus Power Supply has been made, the function to change the setting from the front panel may be disabled via the SpaceLogic C-Bus Commission software to prevent further changes.
The enabled status of the integrated C-Bus Power Supply is shown by the colour of the Unit Indicator.
Refer Unit Indicator for more details.
The state of the network voltage is shown by the state of the C-Bus Indicator.
-
If the C-Bus Indicator is flashing or off, the network voltage is too low, meaning there is insufficient C-Bus power.
-
In this case, additional power supplies may need to be enabled.
-
-
If the C-Bus Indicator is steady, the network voltage is sufficient.
The state of the C-Bus system clock is shown by the colour of the C-Bus Indicator.
| C Bus Indicator | Function |
or (Green or Yellow) |
C Bus clock signal has been detected |
| No C- Bus clock signal has been detected |
Refer C-Bus Indicator for more details.
Enabling/Disabling C-Bus System Clock Generator from the Front Panel
A C-Bus clock signal is required to synchronize communication on the C-Bus Network. The dimmer unit (and most other C-Bus DIN Rail mounted devices) can be configured to generate the C-Bus system clock. It is recommended that the C-Bus system clock generator function be enabled in three units on each network segment.
If a C-Bus system clock is required on the dimmer unit, it can be enabled or disabled from the front panel by performing a short press on the top second-to-right channel button whilst holding down the top left channel button. This toggles the enabled state of the C-Bus system clock generator in the unit.
After the desired setting for the C-Bus system clock generator, the function to change the setting from the front panel may be disabled via the SpaceLogic C-Bus Commission software to prevent further changes.