260422_LSS100500_IHC_Interface_SW

Checking LED Dimmer Functionality

After configuring your LED dimmer channels, it is important to verify that they respond correctly to control commands and provide feedback as expected. You can do this directly from the controller interface by interacting with the KNX group objects assigned to each dimmer.

This process helps confirm that the dimmer is properly linked, that group object mappings are correct, and that feedback is functioning.

To check LED dimmer functionality, proceed as follows:

  1. Open the controller´s Start page and navigate to the Configurator.

  2. Go to the Objects tab and filter the list to locate the group objects assigned to your LED dimmer channel.

  3. Test the objects: For example, find the Status object and change its value from "off" to "on". The corresponding LED dimmer channel should switch on, and you should see updates in the feedback objects within a few seconds.

NOTE: The plugin polls each dimmer channel every 2 seconds to retrieve the current light level. Channels without feedback objects are skipped. If more than 32 dimmer channels are configured, the polling interval may increase to avoid system overload.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.