260422_LSS100500_IHC_Interface_SW

In-Out View

The In-Out view sub-tab provides a comprehensive graphical interface for managing the logical relationships between IHC input and output devices. It is designed to give installers a clear overview of how signals flow through the system.

  • Left panel: Displays editable details of the selected input device, including fields such as Device type, Function, Name, and addressing.

  • Center panel: Shows a visual representation of the input module, IHC Interface, and output module. Inputs and outputs are graphically linked, allowing you to easily trace and manage signal paths.

  • Right panel: Displays editable details of the selected output device, including configuration fields such as Device type, Name, addressing, and reset behavior.

Both input and output devices include a Save changes button at the bottom of their respective panels.

Be sure to save your changes after editing to ensure all mappings are applied correctly.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.