260422_LSS100500_IHC_Interface_SW

Virtual KNX Group Addresses

Virtual KNX group addresses are used for internal communication within the controller and with the IHC interface and Hybrid module.

Format

A virtual group address is a 17-bit integer, with the most significant bit always set to 1, represented in a three-part format:

a/b/c – where each part is a decimal number separated by slashes.

Virtual addresses use the same format as standard addresses but with a different range for the first component.

 

Size (bits)

Range

a

6

32 – 63 (instead of 0 – 31)

b

3

0 – 7

c

8

0 – 255

Addresses with zeroes in one or two components are valid, such as:

  • 32/0/0

  • 63/1/0

  • 42/0/7

Address Range

  • Lowest valid address: 32/0/0

  • Highest valid address: 63/7/255

  • Total possible addresses: 65 536 (32 * 8 * 256 = 65 536)

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.