Introduction
The SpaceLogic IHC Interface is a DIN rail-mounted device designed to work in tandem with the Wiser for KNX/homeLYnk controller (referred to as the controller). It is not a standalone unit. The IHC Interface allows the controller to receive signals from input devices connected to IHC Input modules and to control output devices connected to IHC Output modules. Together, the controller and the IHC Interface effectively replace an IHC Controller version 2 or 3, enabling continued use of the existing IHC wiring and connected devices.
To establish communication between the IHC Interface and the controller, users must install the IHC Plugin, a downloadable application available from the W4K Marketplace. This plugin pairs the IHC Interface with the controller and enables the mapping of IHC addresses to KNX group addresses and vice versa, which is essential for integrating IHC inputs and outputs into the KNX system.
Internally, the controller operates using KNX group addresses, and this mapping allows seamless interaction with devices connected via the IHC modules. Once connected and configured, the system can be reprogrammed to restore most of its original functions. Additionally, it can be expanded with KNX devices or Wiser/Zigbee devices using the SpaceLogic KNX Hybrid module.
With the IHC Plugin, your current IHC installation can be managed through the controller. Integration with Zigbee devices is supported via the KNX Hybrid module, and the entire system can be controlled using the Wiser KNX mobile app.
Limitations and Considerations
-
Functions previously controlled wirelessly via IHC Remote application cannot be re-established directly and must be rebuilt and integrated via KNX and the controller.
-
Room temperature/heating control can be configured via KNX and the controller.
-
The IHC Remote application is not supported and must be replaced by the Wiser KNX mobile application.
-
The IHC Visual and IHC FirmwareLoader applications are not supported.
However, you can import device settings from your existing IHC Visual 3 project into the plugin to facilitate management and migration of your IHC installation.
Prerequisites
Before installing and using the IHC Plugin, ensure the following prerequisites are met:
|
Hardware requirements |
|
|
Software & tools |
|
|
User permissions |
Administrator access to the controller to install applications and perform pairing. |
|
Network & connectivity |
|
|
System preparation |
|
Key Features of the IHC Interface
|
Interface and connectivity |
|
|
Firmware upgrades |
|
|
Device integration |
|
|
Bi-directional communication |
The system supports bi-directional communication across protocols. For instance:
|
|
Resetting and commissioning |
|
|
Interface communication |
|
|
Programming interface |
|