260422_LSS100500_IHC_Interface_SW

PIR Sensor Input Configuration

The corresponding input must be configured to work as a PIR occupancy detector.

Configure the input device as follows:

  • Device type: PIR

  • Function: Occupied / Unoccupied

  • A new KNX group object can be created for the Occupancy input field, or an existing one can be selected.

  • Recommended Min. sending time is 5 seconds. The optimal value depends on the behavior of the connected PIR sensor.

After configuration, the PIR sensor sends occupancy information to the assigned KNX group object, which is then used by the PIR timer and subsequent automations to control lighting behavior.

The figure below shows an example of a PIR input configured in the Input Devices tab of the IHC Plugin, including device type selection, function assignment, and occupancy group object mapping.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.