Toggle Button Configuration
The toggle button used for manual control of the light is configured in a similar way as described in the Toggle Button Functionality section earlier in this user guide.
The main difference in this use case is that only the Status group object is required for basic ON/OFF control.
To configure the toggle button:
-
Open IHC Plugin > DEVICE MAPPING > Input Devices.
-
Select the input connected to the push button.
-
Configure the input as follows:
-
Device type: Push button
-
Function: Toggle (On/Off)
-
-
Assign a Status KNX group object for ON/OFF control.
-
Adjust the Short press time if required.
-
Save the configuration.
The toggle button allows the user to switch the light ON or OFF manually, independently of the PIR sensor state. When activated, the toggle button overrides PIR‑based control until it is pressed again.
The figure below shows an example of a toggle button configuration in the Input Devices tab, including input selection, function assignment, and status group object mapping.