260422_LSS100500_IHC_Interface_SW

Controlling Two Lights with a Single Button

This use case demonstrates how to control two different lights using a single push button by applying short and long press functionality.

Configuration of the Push Button

  1. Open IHC Plugin > DEVICE MAPPING > Input Devices.

  2. Select the input device you want to configure.

  3. Set:

    • Device type: Push button

    • Function: Short / Long press

  4. Assign KNX group objects for:

    • Short press status

    • Long press start status

      Existing group objects can be selected, or new ones can be created using the Add new object option.

  5. Set the following functions:

    • Short press function: TOGGLE

    • Long press start function: TOGGLE

  6. Save the configuration.

Functional Overview

The functional overview is illustrated in the diagram below.

  • A short press of the push button toggles the first light.

  • A long press of the same push button toggles the second light.

Each press type generates a separate status signal, which is mapped to individual KNX group objects and controls a different output device. This allows two independent lights or switches to be controlled using a single physical button.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.