260422_LSS100500_IHC_Interface_SW

Configuring Scene Control for LED Dimmers

Scene functionality is part of the Wiser for KNX controller firmware, using KNX group objects to send predefined values to multiple devices simultaneously.

To begin using scene control with LED dimmers, you first need to create and configure scenes in the controller´s Configurator plugin.

  1. Open the Configurator plugin and navigate to the Scenes tab.

  2. Click Add scene in the bottom-left corner.

  3. In the Scene dialog, enter a unique name for the scene.

  4. Leave Trigger object and Trigger value fields empty (not used in this setup).

  5. Optionally, add Tags to organize and filter scenes.

  6. Click Save to create the scene.

A new scene is successfully created in the Wiser for KNX controller.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.