260422_LSS100500_IHC_Interface_SW

PIR Timer Configuration

The PIR timer is configured in a similar way as the staircase timer described earlier. It is used to switch the light off automatically after a defined time when no occupancy is detected.

Before creating the timer, an additional virtual KNX group object must be created manually:

  • Example: 32/1/6 PIR light demand

  • Data type: 1‑bit (boolean)

This object represents the output of the PIR timer and is later used by automations.

To configure the PIR timer:

  1. In your controller, open Configurator > Timers.

  2. Click Add timer to create a new timer.

  3. Configure the timer parameters.
    The figure below shows an example of a PIR timer configuration, including the trigger object linked to the PIR occupancy input and the target object controlling the light.

  4. Save the configuration.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.