260422_LSS100500_IHC_Interface_SW

Operating elements, terminals

A 2x RJ45

B Inputs 1 ...8

C RS-485 +/-/0 V, SELV

D LED for status indication

E Reset button: for device reset, factory reset, initialization of pairing mode

F Outputs 1 ... 16

G Power Supply DC 24 V

LED for Status Indication

The STATE LED (D) indicates the following conditions:

Operating

 

Meaning

Green, flashing

Normal operation

Power

 

Meaning

Red, flashing

No link available

Red/Orange, flashing

Waiting for DHCP

Red/Green, flashing

Connecting to W4K controller

Pairing

 

Meaning

Orange

You have held down the reset button (E) for 1 to 5 seconds until the LED lights up orange.

Orange, flashing

After pressing the reset button (E) again, the LED starts flashing orange.

Orange, flashing quickly

After selecting the module you want to pair, the LED flashes orange quickly.

Green, flashing 3 times

Pairing was successful.

Red, flashing 3 times

Pairing was not successful or a timeout occurred during the pairing process.

Reset

 

Meaning

Red

Device reset is in progress.

You have held down the reset button (E) for 5 to 10 seconds until the LED lights up red.

Red, flashing

Factory reset in progress.

You have held the reset button (E) for at Red, flashing least 10 seconds and the again for 10 seconds. After releasing the reset button (E), the LED flashes red.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.