260422_LSS100500_IHC_Interface_SW

Understanding Standard/Virtual KNX Group Addresses in the Controller

The controller uses two types of KNX group addresses to manage communication:

  • Standard KNX group addresses

  • Virtual KNX group addresses

Understanding the difference between these types helps determine which to use based on your system configuration.

Choosing Between Standard and Virtual Group Addresses

If you have real KNX devices:

  • Use standard KNX group addresses for communication with commissioned KNX devices.

  • Use virtual KNX group addresses for all other purposes.


If you do not have KNX devices:

  • Use only virtual KNX group addresses.

  • Do not use standard KNX group addresses, as this may cause bus issues and overload the controller.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.