260422_LSS100500_IHC_Interface_SW

Output Devices

The Output devices sub-tab is used to configure and manage all IHC output devices connected to the system. This section allows you to define how each output behaves and how it integrates with the KNX network.

Layout Overview

  • Left panel: Displays a list of all imported or manually added IHC output device mappings. Each device is linked to a specific output module and can be selected for detailed configuration.

  • Center panel: Shows a graphical representation of the IHC output module and the IHC Interface, helping you visualize how outputs are physically connected and routed.

  • Right panel (device details): When a device is selected from the list, its configuration options appear here. You can edit the following fields:

Device Details

  1. Device type: Relay.

  2. Name
    Assign a custom name to the output device for easier identification in your project.

  3. Physical address
    Internally calculated address (range: 0 – 127) representing the device’s physical position in the IHC system.

  4. Logical address
    Indicates the routing of the signal from the IHC Interface to the output module.

  5. After reset (On/Off/Persistent)
    Defines the default state of the output after a system reset.

  6. Select object
    This option allows you to associate the IHC input device with a KNX object.
    You can select an already created object or you can create a new one.
    Once you click on Add new object, new window will appear.
    Here you can set the name of the object, comments, units, and specify whether it is a Virtual KNX object.

Once you have configured an output device, click Save changes to apply and store your settings.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.