Device Mapping
The DEVICE MAPPING tab in the IHC Plugin interface provides a centralized view for managing the connection between your IHC devices and the controller. This section is essential for assigning and organizing how input and output signals from the IHC system are interpreted and controlled within the KNX environment.
The tab is divided into three sub-sections:
-
Input devices: For mapping IHC input device addresses to corresponding KNX group addresses for devices such as push buttons, sensors, and binary inputs.
-
Output devices: For mapping of KNX group addresses to corresponding IHC output device addresses for devices like lights, fans, or other actuators.
-
In-Out viewFor visualizing and editing the logical connections between input and output devices in a single, integrated interface.
-
RS485 (Dimmers): For configuring dimming devices connected via the RS485 interface, such as 2-channel LED dimmers.
Each sub-tab allows you to view and edit connected devices, assign names, configure port mappings, and ensure proper communication between the IHC system and the controller. This structured approach simplifies commissioning and ensures a seamless integration of IHC devices into your smart home or building automation setup.