260422_LSS100500_IHC_Interface_SW

Workflow

This overview shows the sequence of the entire process of commissioning the SpaceLogic IHC Interface up to integration with IHC Plugin.

  1. Connect your SpaceLogic IHC Interface to the controller.

  2. Login to controller.

  3. Download IHC Plugin.

  4. Open IHC Plugin.

  5. Pair your SpaceLogic IHC Interface with the controller.

  6. Import existing IHC project into IHC Plugin.

  7. Fine-tune the settings in the Device mapping tab of the IHC Plugin.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.