260422_LSS100500_IHC_Interface_SW

Scene Recall Functionality

To define what happens when a scene is recalled:

  1. Click the sequence icon in the Sequence column of your scene.

  2. Click Add objects to include KNX group objects in the scene.

  3. The Add objects dialog appears, where you select multiple group objects to be part of the scene. Use the filter to locate relevant objects (e.g., those containing “level”).

  4. Select all group objects you want to include in the scene (e.g., all LED dimmer level objects) and click Save.

  5. Assign values to each object: Click the set value icon in the Set value column of the value.

  6. In the Set object value dialog, set value from 0 to 100, where 0 = OFF and 100 = full brightness. Click Save.

  7. To test the scene, click Run scene in the Sequence for scene dialog.

The scene is fully configured to recall predefined brightness levels for selected LED dimmer channels. When the scene is activated, the assigned values are sent to all included KNX group objects, instantly adjusting the lighting to the desired state.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.