260422_LSS100500_IHC_Interface_SW

IHC Plugin Installation

To begin using the IHC Plugin, you must first install it on your controller. The plugin is available through the controller’s Marketplace.

Follow the steps below to complete the installation process:

  1. Log in to the controller through your web browser.

  2. Click on in the top right corner to open the Marketplace.

  3. Click on the green bar in the middle to display the applications available for installation under Install new apps and widgets

    .
  4. From the list of available applications, select the IHC Plugin and click on the right to start the installation.

  5. Return to the Start page of your controller in the web browser. The installed IHC Plugin will appear among other applications:

  6. Click on the IHC Plugin icon to open the plugin:

NOTE: It is recommended to enable the plugin's automatic update to ensure you always have the latest version.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.