Scenes for the Light Level Control
To control different lighting levels depending on the situation and time of day, separate scenes are used.
Create three scenes with predefined light levels, for example:
-
PIR high – light level set to 100 %
-
PIR low – light level set to 25 %
-
PIR off – light level set to 0 %
To create the scenes:
-
In your controller, open Configurator > Scenes.
-
Click Add scene to create a new scene and assign a descriptive name (e.g. PIR high).
-
Add the relevant level group object of the LED dimmer to the scene.
-
Set the required brightness value.
-
Save the scene.
-
Repeat the same steps for the remaining scenes (PIR low and PIR off).
These scenes are later recalled by automations to apply the correct light level based on PIR activity, manual control, and time conditions.
The figure below shows an example of scene configuration in the Scenes tab, including predefined brightness values for the selected LED dimmer channel.