260422_LSS100500_IHC_Interface_SW

Device and Factory Reset

If your IHC Interface does not respond as expected, you can perform a reset. There are two types of reset: device reset and factory reset.

Device Reset

A device reset reboots the IHC Interface without erasing configuration or commissioning data. This is useful for resolving temporary issues while keeping all settings intact.

To perform a device reset:

  1. Press and hold the reset button (E) for 5 to 10 seconds until the STATE LED lights up red.

  2. Release the button. The device will restart and resume normal operation.

Factory Reset

A factory reset restores the IHC Interface to its original factory settings. All configuration data, commissioning information, and logs are erased. After a factory reset, you must reconfigure and pair the device again.

To perform a factory reset:

  1. Press and hold the reset button (E) for at least 10 seconds, then press and hold it again for 10 seconds.

  2. Release the button. The STATE LED will flash red, indicating that the factory reset is in progress.

Important Notes

  • Use device reset for troubleshooting without losing configuration.

  • Use factory reset only when reconfiguration is required or if pairing cannot be restored.

  • After a factory reset, default network settings (DHCP enabled) are applied.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.