260422_LSS100500_IHC_Interface_SW

Standard KNX Group Addresses

Standard KNX group addresses are used to communicate with real KNX devices connected to the KNX bus. These devices must be properly configured and commissioned using ETS.

Format

A standard KNX group address is a 16-bit integer, represented in the format:

a/b/c – where each part is a decimal number separated by slashes:

 

Size (bits)

Range

a

5

0 – 31

b

3

0 – 7

c

8

0 – 255

The address 0/0/0 is not allowed.

However, addresses with zeroes in one or two components are valid, such as:

  • 0/0/1

  • 2/0/0

  • 0/3/0

  • 0/4/5

  • 6/0/7

  • 8/1/0

Address Range

  • Lowest valid address: 0/0/1

  • Highest valid address: 31/7/255

  • Total possible addresses: 65 535 (32 * 8 * 256 – 1 = 65 535)

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.