260422_LSS100500_IHC_Interface_SW

Creating KNX Objects in the Controller

To use KNX group addresses, you must first create an object.

Detailed instructions are available in the Configurator – Main Page > Objects > Add New Object chapter of the Controller User Guide. This chapter also includes additional helpful information.

Steps to Create an Object

  1. Navigate to: Start page of your controller > Configurator > Objects tab.

  2. Click Add New Object.

  3. Choose one of the following options:

    • Create standard object

    • Create virtual object

This opens the Add New Object dialog.

Group Address Field

  • The Group address field will be automatically filled with the next available KNX group address (standard or virtual, depending on your selection).

  • You can accept the suggested address or enter a custom one.

  • The address must be unique. If already in use:

    • The field is underlined in red.

    • A red circle icon appears next to the field.

    • Hovering over the icon displays: This address is already in use.. Choose a different address and try again.

NOTE: The group address cannot be changed later. To use a different address, create a new object.

Required Fields

Three mandatory fields must be filled:

  • Group address

  • Object name

  • Data type

Object Name

  • Must be unique.

  • If already in use:

    • The field is underlined in red.

    • A red circle icon appears.

    • Hovering over the icon shows: This name is already in use.. Choose a different name and try again.

  • The object name can be changed later.

Data Type

  • If unsure, select a data type that seems appropriate.

  • The data type can be changed later.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.