260422_LSS100500_IHC_Interface_SW

Short/Long Press Functionality of a Push Button

Short/long press functionality has been implemented for push buttons. This functionality extends standard button operation and allows a single push button to control multiple actions depending on the press duration.

Short and long press functionality can be used in various use cases, for example:

  • Controlling two different lights or switches using short press and long press of the same button.

  • Controlling a single light with a short press and recalling a scene with a long press.

  • Creating “Follow” functionality using a long press start and long press stop.

This section describes how to configure push buttons with short/long press functionality and provides several practical configuration examples.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.