260422_LSS100500_IHC_Interface_SW

Scene Store Functionality

Scene store functionality allows saving the current LED Dimmer levels into a scene.

To enable this:

  1. Click the sequence icon in the Sequence column of your scene.

  2. For each object in the scene sequence you want to edit, click its row in the Sequence for scene dialog.

  3. In the Edit object dialog, select the appropriate level feedback object in the Status object field. Use filtering to find the correct object.

  4. Click Save to apply changes.

  5. Repeat for all objects in the sequence.

The scene is prepared to store the current brightness levels of the selected LED dimmer channels. When the store command is triggered, the scene will capture and save the real-time values from the assigned feedback objects, allowing accurate recall later.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.