DOCA0271EN-00

Energy

The Avatar_Energy function block returns the status of the acyclic energy data of the specified avatar.

Avatar_Energy Function Block

Avatar_Energy Output Interface

Output

Data Type

Description

InstActivePower

DINT

Total active power for the avatar. (Unit: W)

MaxActivePower

DINT

Maximum value of the active power for the avatar. (Unit: W)

MaxActivePowerTimestamp_Y

DINT

Date and time when the maximum active power value was recorded.

MaxActivePowerTimestamp_M

SINT

MaxActivePowerTimestamp_D

SINT

MaxActivePowerTimestamp_h

SINT

MaxActivePowerTimestamp_min

SINT

MaxActivePowerTimestamp_sec

SINT

MaxActivePowerTimestamp_cs

SINT

InstReactivePower

DINT

Total reactive power for the avatar. (Unit: VAR)

MaxReactivePower

DINT

Maximum value of the reactive power for the avatar. (Unit: VAR)

MaxReactivePowerTimestamp_Y

DINT

Date and time when the maximum reactive power value was recorded.

MaxReactivePowerTimestamp_M

SINT

MaxReactivePowerTimestamp_D

SINT

MaxReactivePowerTimestamp_h

SINT

MaxReactivePowerTimestamp_min

SINT

MaxReactivePowerTimestamp_sec

SINT

MaxReactivePowerTimestamp_cs

SINT

PowerFactor

SINT

True power factor value.

MinPowerFactor

SINT

True minimum power factor value.

MaxPowerFactor

SINT

True maximum power factor value.

MinPowerFactorTimestamp_Y

DINT

Date and time when the minimum power factor value was recorded.

MinPowerFactorTimestamp_M

SINT

MinPowerFactorTimestamp_D

SINT

MinPowerFactorTimestamp_h

SINT

MinPowerFactorTimestamp_min

SINT

MinPowerFactorTimestamp_sec

SINT

MinPowerFactorTimestamp_cs

SINT

MaxPowerFactorTimestamp_Y

DINT

Date and time when the maximum power factor value was recorded.

MaxPowerFactorTimestamp_M

SINT

MaxPowerFactorTimestamp_D

SINT

MaxPowerFactorTimestamp_h

SINT

MaxPowerFactorTimestamp_min

SINT

MaxPowerFactorTimestamp_sec

SINT

MaxPowerFactorTimestamp_cs

SINT

TotalActiveEnergy

DINT

Total active energy value for all avatars in the system with Energy Monitoring Enabled. (Unit: Watt-hours)

TotalActiveEnergy_O

BOOL

Total active energy overflow value for all avatars in the system with Energy Monitoring Enabled.

TotalReactiveEnergy

DINT

Total reactive energy value for all avatars in the system with Energy Monitoring Enabled. (Unit: VAR-hours)

TotalReactiveEnergy_O

BOOL

Total reactive energy overflow value for all avatars in the system with Energy Monitoring Enabled.

ActiveEnergyChannel1

DINT

Channel 1: ToU (Time of Use) total active energy value.

ActiveEnergyChannel1_O

BOOL

Channel 1: ToU (Time of Use) total active energy overflow value.

ActiveEnergyChannel2

DINT

Channel 2: ToU (Time of Use) total active energy value.

ActiveEnergyChannel2_O

BOOL

Channel 2: ToU (Time of Use) total active energy overflow value.

ActiveEnergyChannel3

DINT

Channel 3: ToU (Time of Use) total active energy value.

ActiveEnergyChannel3_O

BOOL

Channel 3: ToU (Time of Use) total active energy overflow value.

ActiveEnergyChannel4

DINT

Channel 4: ToU (Time of Use) total active energy value.

ActiveEnergyChannel4_O

BOOL

Channel 4: ToU (Time of Use) total active energy overflow value.

ReactiveEnergyChannel1

DINT

Channel 1: ToU (Time of Use) total reactive energy value.

ReactiveEnergyChannel1_O

BOOL

Channel 1: ToU (Time of Use) total reactive energy overflow value.

ReactiveEnergyChannel2

DINT

Channel 2: ToU (Time of Use) total reactive energy value.

ReactiveEnergyChannel2_O

BOOL

Channel 2: ToU (Time of Use) total reactive energy overflow value.

ReactiveEnergyChannel3

DINT

Channel 3: ToU (Time of Use) total reactive energy value.

ReactiveEnergyChannel3_O

BOOL

Channel 3: ToU (Time of Use) total reactive energy overflow value.

ReactiveEnergyChannel4

DINT

Channel 4: ToU (Time of Use) total reactive energy value.

ReactiveEnergyChannel4_O

BOOL

Channel 4: ToU (Time of Use) total reactive energy overflow value.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.