DOCA0271EN-00

Import the TeSys™ island Module

Import the TeSys island module to the Ethernet bridge. This file uses the following naming convention: {DeviceName}Module.L5X.

After import, the device shows up in the I/O configuration tree and the Controller Tags section of the project.

Once the module exists, define the target IP address of the device.

NOTE: If you skip this step before importing the Subroutine and AOI, you will be required to manually set the target communication path for each Acyclic function block.

Define the IP Address

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.